CAN2ETH:Plugins issues: Cannot load configuration Llce_Af/CAN_43_LLCE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN2ETH:Plugins issues: Cannot load configuration Llce_Af/CAN_43_LLCE

1,993 Views
Jitender1203
Contributor III

Hi ,

We are working on CAN2ETH/ETH2CAN project, we took the NXP reference project from LLCE-1.0.4: and we are reffereing AN13423 document for this project.

SW packages details :

  1. EBTresos 29.0.2
  2. S32G_LLCE_1_0_4
  3. SW32G_RTD_4.4_3.0.2_HF01
  4. PFE-DRV_S32G_M7_MCAL_BETA_0.9.7

Once the Project is imported (C:NXP\S32_LLCE_1_0_4\sample_app_llce_llce_sample_app_pfe\tresos_S32G2), then after load configuration, we are getting the error Cannot load configuration Llce_Af. Another module already created a configuration at /AUTOSAR/TOP-LEVEL PACKAGES/Llce_Af/ELEMENTS/Llce_Af.

screenshot is also attached.

 

error.jpg

0 Kudos
Reply
2 Replies

1,771 Views
mmoi
Contributor II
I have same error  error Cannot load configuration Llce_Af. Another module already created a configuration at /AUTOSAR/TOP-LEVEL PACKAGES/Llce_Af/ELEMENTS/Llce_Af.
Have you solved your problem?
0 Kudos
Reply

1,977 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We are not seeing the same behavior you are seeing. Below our results:

DanielAguirre_0-1680200135224.png

The only question we have is if you have the needed plugins under the "C:/EB/tresos/plugins"?

You should have all the RTD/LLCE plugins inside this folder.

Please, let us know.

0 Kudos
Reply