CAN Devices Enter Busoff State After Wakeup In S32G2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN Devices Enter Busoff State After Wakeup In S32G2

3,246件の閲覧回数
shuangjunzhu
NXP Employee
NXP Employee

Hi Experts,
Customer encounter an issue. While the S32G M7 core is wakeup from sleep state, it will execute the same process as the cold-start for power-up. 

The LLCE can2can routing is enabled. Before sleep, the CAN network is working well.

Usually, the CAN devices will report BUSOFF error once the M7 core re-enable the BCAN controller in wakeup (same as power-on) process.

Please help to review whether the initiation sequence of LLCE MCAL driver rightly cover this kind of corner case.

Thanks,

Jeff

0 件の賞賛
返信
2 返答(返信)

3,227件の閲覧回数
bpe
NXP Employee
NXP Employee

Can you please update this thread with the following information:

 

  1. The version of LLCE FW/driver package you are using
  2. If the behaviour described in your post was observed on an NXP reference or development board or it is a custom design.

Best Regards,
Platon

 

0 件の賞賛
返信

3,217件の閲覧回数
shuangjunzhu
NXP Employee
NXP Employee

It's 1.0.0 firmware and driver for MCAL.

The failure is observed on customer's board.

0 件の賞賛
返信