Build the s32g3 series linux bsp environment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build the s32g3 series linux bsp environment

646 Views
112233aabbcc
Contributor I

The environment cannot access the code in the GitHub download repository, and there is an error. Is there anyone who can help?

Tags (1)
0 Kudos
Reply
1 Reply

640 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @112233aabbcc 

Thanks for the post.

Would you mind providing us more information about the building failure?

Which version BSP you are working with? would you mind showing whole steps for the Yocto environment preparation and building, including every command used and output from them would be preferred.

 

BR

Chenyin

0 Kudos
Reply