Boot OS for GOLDBOX & compiler tool chain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot OS for GOLDBOX & compiler tool chain

1,767 Views
vinayakaghor13
Contributor I

Hello,

I am planning to buy GOLDBOX. I want to use this for ethernet to CAN gateway. I want to know

1. Is OS ready available?

2. Whether compiler tool chain available? Can we install this our machine?

3. I have seen GUI to download use cases in one of video. What is GUI used to download use cases? where it is available?

Kindly reply.

Vinayak

Tags (1)
0 Kudos
Reply
1 Reply

1,751 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Vinayakaghor13,

 

1. Yes, Linux BSP is available to download.

2. You can integrate the S32 design is you want.

3. is the flash tool burn image is used by S32 design tool.

 

Regards

0 Kudos
Reply