BSP31 points to invalid pfeng driver repo commit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BSP31 points to invalid pfeng driver repo commit

ソリューションへジャンプ
3,520件の閲覧回数
f_frank
Contributor I

After upgrading from BSP30 to recently released BSP31 for S32G, the pfe recipe points to a not (yet) committed revision in pfeng repository. Same unreleased revision is also referenced by libfci_0.9.6.bb.

Am I missing some step here or is the driver not yet released to that repo. What is the timeline to commit it?

@jpetrous tagging you since most commits in pfeng repo were done by you.

タグ(3)
0 件の賞賛
返信
1 解決策
3,513件の閲覧回数
bpe
NXP Employee
NXP Employee

Automotive BSP 31 has not been officially released. Early code drops currently available
through GIT repositories may have certain issues. Full support in the Community
will be available when the official BSP 31 release is made. Until then, our
main recommendation is, stay with BSP 30.0. A limited support to BSP 31 code
drops can be requested via tickets, our answers depend on availability of the SW development
team members for internal discussion.

Best Regards,
Platon

 

元の投稿で解決策を見る

2 返答(返信)
3,368件の閲覧回数
lakehu
Contributor II

When bsp31 could have a official open release with PFE ??

Thanks 

0 件の賞賛
返信
3,514件の閲覧回数
bpe
NXP Employee
NXP Employee

Automotive BSP 31 has not been officially released. Early code drops currently available
through GIT repositories may have certain issues. Full support in the Community
will be available when the official BSP 31 release is made. Until then, our
main recommendation is, stay with BSP 30.0. A limited support to BSP 31 code
drops can be requested via tickets, our answers depend on availability of the SW development
team members for internal discussion.

Best Regards,
Platon