AI models integration on NXP hardware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AI models integration on NXP hardware

1,017件の閲覧回数
mohamedtalal
Contributor I

Hi,

I might be asking a generic question to most of you, but I'm little bit new to the community of NXP

If i have an AI model that perform some task of classification, I want to know how to integrate this AI model to the NXP hardware.

Does NXP even support this integration?

Thank you.

0 件の賞賛
返信
1 返信

992件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @mohamedtalal 

Thank for you post.

May I know if you are willing to use your AI model on S32G2/3 platforms? since this board is targeted to the S32G products.

If so, NXP provided the Yocto BSP for the S32G platforms, while Linux could run on the platform, so that it is possible for running common AI software packages like Tensorflow or so, but it is not within our support scope from this channel, I apologize.

I suggest contacting your DFAE/FAE/sales for further information on this field.

 

BR

Chenyin