ADC with DMA, without interrupts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC with DMA, without interrupts

1,294 Views
Radish_44
Contributor I

Hi!

Could please provide an example project for S32g274, where the ADC in configured to run in DMA mode,with continuous mode, without interrupt?

 

Thanks!

Labels (1)
0 Kudos
Reply
1 Reply

1,248 Views
nxf92355
NXP Employee
NXP Employee

Hi Mate Sziak

 

Thanks for using NXP community. Hope you are doing well

Sorry , There are no same example available on nxp site or with RTD. there are example available is Adc Driver by Interrupt and DMA Transfer.

 

Regards ,

Tushar

0 Kudos
Reply