User Space Hash Example Based on LIBHSE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

User Space Hash Example Based on LIBHSE

User Space Hash Example Based on LIBHSE

Recently, there are several customers who feel interests in developing applications in Linux user space to directly use the HSE, in order for behaving hardware based encryption and authentication. The customers need direct examples for their development reference, however, from the source code released in formal BSP, there are only simple encryption examples existed, they need other kinds of examples, for example, hash operations.

This reference document describes access schemes to the HSE using the LIBHSE standard API. It shows a hash operation example of using LIBHSE to access the HSE under incorporation of the NXP Linux BSP software.

A sample application is implemented taking use of the APIs provided by LibHSE:

chenyin_h_0-1748328615576.pngchenyin_h_0-1748328615576.png

 

Reference the attached PDF file for details.

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎06-04-2025 08:28 PM
更新者: