User Space Hash Example Based on LIBHSE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

User Space Hash Example Based on LIBHSE

User Space Hash Example Based on LIBHSE

Recently, there are several customers who feel interests in developing applications in Linux user space to directly use the HSE, in order for behaving hardware based encryption and authentication. The customers need direct examples for their development reference, however, from the source code released in formal BSP, there are only simple encryption examples existed, they need other kinds of examples, for example, hash operations.

This reference document describes access schemes to the HSE using the LIBHSE standard API. It shows a hash operation example of using LIBHSE to access the HSE under incorporation of the NXP Linux BSP software.

A sample application is implemented taking use of the APIs provided by LibHSE:

chenyin_h_0-1748328615576.pngchenyin_h_0-1748328615576.png

 

Reference the attached PDF file for details.

Labels (1)
Attachments
No ratings
Version history
Last update:
‎06-04-2025 08:28 PM
Updated by: