undefined reference to `fopen'

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

undefined reference to `fopen'

6,175件の閲覧回数
jeffqin
Contributor I

Hi, dears:

   I use S32DS to open an file, but when compile it shows:"undefined reference to `fopen'".

 My GCC is: S32K144 RTM SDK for GCC.

C project. No OS. And use S32DS "project ->build all" to build.

What should I do to fix this?

Thanks!

My code:

#include <stdio.h>

......

fp = fopen("BAP3_PATCH_SC58579_ROM_7_2.bin","rb");

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

5,300件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Jeff, 

the fopen function is not implemented. S32K144 is small device and normally doesn't use file system. If you implemented file system - you also need implement fopen and other file I/O functions.  

Anyway - what are trying to do with fopen in your project? 

Jiri 

0 件の賞賛
返信

5,300件の閲覧回数
jeffqin
Contributor I

Hi Jiri:

   Thanks, then does it mean it is difficult or lots of work needed to be done? If so, I can use other method to do this work.

In my project, there is another chip: TDF8534, we need to update TDF8534 with patch file named:"*.bin", this file will be different when a new version release. So if I can use file system, there will be less risk to replace this file only, more risk to copy the data using other editor.

0 件の賞賛
返信

5,300件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Jeff, 

I don't know your design - in case that you have connected some SD card or any other memory/drive to S32K144, implementing file system is good idea. If there is no external memory/drive - easier way is transfer .bin file from PC by UART or by any other communication channel. 

Jiri

0 件の賞賛
返信

5,300件の閲覧回数
jeffqin
Contributor I

Hi Jiri:

   Thanks!

0 件の賞賛
返信