s32k1 sdk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k1 sdk

17,732 Views
Anjalipurushothaman
Contributor III

 

while creating a new s32ds application project, while selecting tool chain(NXP GCC 9.2 FOR Arm 32-bite bare metal) , following next button and selecting the cores and parameters (SDK IS NOT SHOWING).

Whereas while selecting NXP GCC 6.3 for Arm , SDK options are available(free master_s32k144, s32k144_sdk) 

Labels (1)
0 Kudos
Reply
9 Replies

17,677 Views
Anjalipurushothaman
Contributor III

Still the same , SDK is not showing while creating new application project specifically for  (while selecting tool chain(NXP GCC 9.2 FOR Arm 32-bite bare metal).

 

 

0 Kudos
Reply

17,677 Views
Anjalipurushothaman
Contributor III
 
0 Kudos
Reply

17,665 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Anjalipurushothaman 

Some issues have been reported with S32K1 support in S32DS v3.5, at this moment we recommend for the S32K1 family use the S32DS v3.4 since it has support for the latest version of SDK (4.0.3) and RTDs (1.0.1) available for the family.

Sorry for the inconvenience.

 

 

0 Kudos
Reply

17,645 Views
Anjalipurushothaman
Contributor III

Thanks, Let me try with the earlier version then.

 

Also would like to know do I need to install VDK? Also to know where I can install the versions of Synopsys Virtualizer Studio and VDK packages .

Please do share the link for S32 Design Studio for S32 Platform 3.4 Release Notes

0 Kudos
Reply

17,621 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Anjalipurushothaman 

You can consult the release notes of S32DS v3.4 at the below link:

S32 Design Studio 3.4 – Windows/Linux -> S32 Design Studio IDE -> Previous tab.

Regarding Synopsys Virtualizer Studio and VDK packages please get in touch with Synopsys for further support in this part.

NXP S32 Automotive Processing Platform

0 Kudos
Reply

17,692 Views
Anjalipurushothaman
Contributor III
 
0 Kudos
Reply

17,722 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Anjalipurushothaman 

Which S32DS version are you using?

Also, could you share an image of your Installation Details?

 

B.R.

VaneB

0 Kudos
Reply

17,694 Views
Anjalipurushothaman
Contributor III

The latest version of S32DS 3.5,

0 Kudos
Reply

17,688 Views
SivaB
Contributor III

Hi,

Install and try the below latest RTD version.

S32K1 Real-Time Drivers Version 1.0.1 HotFix 01.

 

0 Kudos
Reply