What Java version for S32 Design Studio for Arm 2018.R1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What Java version for S32 Design Studio for Arm 2018.R1

1,791 Views
alwin_lutz
Contributor II

I fixed on problem and created a new.  Here it goes:

The new installation of Integrity failed because of a conflict with the Java version on my laptop.

So the IT request was to remove that Java version.  I did that and Integrity installed.

After that my NXP Studio 2018.R1 gives me a message that it failed to load the JNI shared library "...\jvm.dll".  I checked that path and the file is there, but no success.

So here is my question:

Can I install a Java version that will make the Design Studio work again or do I need to do a complete new install?

 

Any help appreciated.

 

Regards,

Alwin

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,781 Views
JRoberto
NXP TechSupport
NXP TechSupport

Hello @alwin_lutz 

Personally, I would reinstall the complete IDE in order to avoid additional hidden wrong configurations.

Best Regards!

0 Kudos
Reply