S32R458 Premium Radar SDK Evaluation Package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R458 Premium Radar SDK Evaluation Package

2,177 Views
CSBoy
Contributor II

Hi,

I used the installation package  is [S32r45_premium_Radar_SDK_evaluation_Package_0_8_0_220519.exe]

After installation, the build and project directories could not be found in each module of the PRSDK Algorithm. For example [TFDT Algorithm]

CSBoy_0-1659323918701.png

But, in the PRSDK_User_Manual file,Mention that users can compile and import projects,

CSBoy_1-1659324212114.pngCSBoy_2-1659324301483.png

 

 

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

2,166 Views
HaoRen
NXP Employee
NXP Employee

Hi,

I have tested several recently updated installation packages, but there is no installation problem you mentioned. Please confirm whether you added the license file during installation, or download the latest package to test again.

nxf47389_0-1659405263357.png

 

nxf47389_1-1659405279353.png

 

 

0 Kudos
Reply

2,157 Views
CSBoy
Contributor II

hi,

I have compared your pictures, which are different from the installation package I downloaded. Mine is [S32r45_premium_Radar_SDk_evaluation_Package_0_8_0_220519.exe], and the size of the installation package is 74318KB.  So, where can I download the [S32R45_Preminum_Radar_SDK_080_220610] installation package.

thanks

Tags (1)
0 Kudos
Reply

2,151 Views
HaoRen
NXP Employee
NXP Employee

PRSDK is a paid software package.

The evaluation package is different from the complete package.

Could you tell me which customer you are?   This requires market support

0 Kudos
Reply

2,129 Views
CSBoy
Contributor II

Thank you.  if necessary, I'll contact nxp market.

0 Kudos
Reply