S32K148 LWIP RTM v3.0.0 example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 LWIP RTM v3.0.0 example

1,859件の閲覧回数
liuweiliang
Contributor II

example:lwip_s32K148

I'll look at the code for this example,I have ported LWIP protocol on 5748 before,In contrast, there are some questions。

When self-porting, the interface corresponding to the low driver is:low_level_output 、low_level_input、low_level_input.  in function low_level_input,Initializing a network adapter.but int the lwip_S32k148,i just found function: 'enetif_low_level_output'、'enetif_low_level_init',don't found about filed ' low_level_input'? where do i found this function.

i check help doc 'lwip_s32k148_group.html',but hasn't any introduce.

in this example, enet recevie data ,dose trigger interrupt? 

I want use MQTT protocal,dose has any example?

タグ(1)
0 件の賞賛
返信
0 返答(返信)