S32K SDK for IAR IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K SDK for IAR IDE

2,154件の閲覧回数
hansonhe
NXP Employee
NXP Employee

Dear, 

We have S32K SDK for S32DS IDE, whether we have SDK package for IAR IDE? Thanks.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,598件の閲覧回数
robertboys
Contributor IV

Hello

Keil MDK has this SDK installed as part of the S32K-144 Software Pack:  See attachment.

All you need to do is click on the component you want and it is inserted into your project along with any other files needed.

We are working on S32K-148 at this time.

The eval version of MDK can be used to evaluate and use the SDK (for < 32K).

Bob Boys

0 件の賞賛
返信

1,598件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

unfortunately, SDK package is for S32 Design Studio only.

Regards,

Martin

0 件の賞賛
返信