S32 design studio SDK error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 design studio SDK error

2,688件の閲覧回数
kbj
Contributor IV

Hi,

I develop with S32K144 EVB.

I use S32 design studio for ARM.2014.R1 and S32K144_SDK_gcc version 0.8.6.

I configured pin_mux and clock_manager and then generate code.

At first, source code was generated.

I added some code and changed pin configuration and then generate code.

But At second, source code was not generated with below error code.

How to resolve this problem?

1.PNG

Best regards,

Byungju.

2 返答(返信)

2,437件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share your project? It looks like that there is issue for accessing files on your system. Isn't your main.c opened in different editor which makes this file read-only? 

Jiri

2,437件の閲覧回数
kbj
Contributor IV

Hi,

I use s32k144 EVB.

We use s32k144 next project. so I pre-develop with s32k144EVB.

I found to solve this problem.

Clicking the reload project solve the problem. 

But I don't know why the problem is occured.

1.PNG

Thanks for your support.

Best regards,

Byungju.

0 件の賞賛
返信