OsIfSystemTimerClockRef must be enabled in baremetal mode detailed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OsIfSystemTimerClockRef must be enabled in baremetal mode detailed

1,761件の閲覧回数
harryoceana
Contributor II

Use EB tresos 29, OsIfSystemTimerClockRef, It's not editable,The MCU clock is the default, What should I do to change this option?

 

捕获.PNG

捕获1.PNG

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,715件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Click icon to enable the container. Will you be able to select OsIfSystemTimerClockRef ?

OsIfSystemTimerClockRef.PNG


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信