Not able to generate code from Processor Expert file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to generate code from Processor Expert file

2,462件の閲覧回数
amarjeet_kumar
Contributor II

Hi All

When I am Creating S32 DS Application project and selecting toolchan (Standard S32DS toolchain for ARM) with SDK (S32SDK_S32K14x_EAR_0.8.6) then I am able to generate processor expert code by keeping only SOSC_CLK.

 

Below is Configuration snapshot for the reference.

1.PNG

But When I am Creating S32 DS Application project and selecting toolchan (IAR Toolchain for ARM - (8.x)) with SDK (S32SDK_S32K1xx_RTM_3.0.0) then I am not able to generate processor expert code by keeping only SOSC_CLK.

 

Below is Configuration snapshot for the reference

Error Snapshot:

Please help me in solving this clock configuration problem.

Thanks

Amarjeet

0 件の賞賛
返信
3 返答(返信)

2,347件の閲覧回数
razva_tilimpea
NXP Employee
NXP Employee

Hi,

Please re-upload last 2 snapshots. I see just some blanks.

Razvan

0 件の賞賛
返信

2,348件の閲覧回数
amarjeet_kumar
Contributor II

Hi Razvan

Please find here the 2 snapshots.

Configuration snapshot for the reference

1.jpg

Error Snapshot:

2.jpg

Thanks

Amarjeet

0 件の賞賛
返信

2,347件の閲覧回数
razva_tilimpea
NXP Employee
NXP Employee

Thanks,

Based on that error and would like to know how did you imported the project? It's a project started with EAR 0.8.6 and after that you switched the same project to RTM 3.0.0?

Could you provide me the steps to reproduce it on my side?

Best regards,

Razvan

0 件の賞賛
返信