NXP MPC5748 Tcpip Stack component does not include

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP MPC5748 Tcpip Stack component does not include

1,637件の閲覧回数
pratikj_panchal
Contributor I

Hello,
I've a MPC5748 DevKit and I'm working in Ubuntu 18(x64).
IDE: S32 Design Studio.
In this IDE when I was add tcpip stack component then tcpip stack not include.

and got a following error :

tcpipstack_componet_error.png

and I'm working in Core : Z4_0.

Kindly tell what should I do for add tcpip stack component into my current project ?

Thanks & Regards,
Pratik Panchal

0 件の賞賛
返信
1 返信

1,550件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

based on release notes - SDK is fully supported on Windows host only. Under linux some components aren't working properly. 

Jiri

0 件の賞賛
返信