MPC5746C Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5746C Interrupt

1,584件の閲覧回数
huaqingren
Contributor I

I develop MPC5746C with S32DS and SDK, but in the project I have configured, I can't find the files such as "flashrchw.c", "intc_sw_handlers.S", "intc_SW_mode_isr_vectors_MPC574xC.c", "MPC57xx__Interrupt_Init.c", "Vector.c". How to get this files in the SDK or how to configure it?

ラベル(1)
0 件の賞賛
返信
1 返信

1,480件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello,

the project structure is a bit different when project is created with SDK enabled. Please check the Startup_Code folder in your project:

stanish_0-1698314447685.png

 

flashrchw.c is basically implemented in startup_MPC5746C.s where RCHW is defined.

intc_sw_handlers.s exception handlers are implemented in  core0_intc_sw_handlers.s

intc_SW_mode_isr_vectors_MPC574xC.c  is defined in startup_MPC5746C.s see label __isr_vector:

MPC57xx__Interrupt_Init.c is partially implemented in S32_core_e200.h

Vector.c has been transfered into interrupt_vectors.s 

 

Please check the files and let us know which specific function you are missing or what is your goal.

This will help us to resolve the issue much faster.

Thanks!

Stan

0 件の賞賛
返信