MPC5744P SPI 32bit/frame SPI_PAL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5744P SPI 32bit/frame SPI_PAL

5,221 次查看
838927242
Contributor II

I  transmit 16bit/frame SPI  with SPI_PAL ,no problem heppend;

but when I try to transmit 32bit/frame SPI  the initialization can not pass.

who can help solve the problem.... thanks

标签 (1)
0 项奖励
回复
1 回复

5,047 次查看
razva_tilimpea
NXP Employee
NXP Employee

Hi,

On this CPU are supports native maximum 16 bits frame.

You can workaround this by using continuous mode to keep SS low during 2 frames of 16 bits.

Best regards,

Razvan