H.264 Hardware Encoder support on S32V234

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

H.264 Hardware Encoder support on S32V234

1,587 Views
muhammad_nadeem
Contributor I

Hi,

 

We are developing an application to capture videos and want them to encode using H.264 hardware encoder in lossless mode on S32v234. I wonder if the HW H.264 Encode support lossless mode? and where can I find APIs and sample code to utilize hardware encoding. Any pointer will be really appreciated.

-- Muhammad Nadeem

Labels (1)
0 Kudos
Reply
1 Reply

1,542 Views
bpe
NXP Employee
NXP Employee

Please be aware, that support to S32V234 Vision subsystem modules is done only
via tickets. This Community is not appropriate for questions of this kind. I
will contact you by e-Mail with respect to this issue, for future requests,
please use only tickets.

 
Have a great day,
Platon

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply