Flash DRV erasesector in SDK s32k1xx 15 does not execute correctly

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash DRV erasesector in SDK s32k1xx 15 does not execute correctly

1,196 次查看
561999181
Contributor I

Flash DRV erasesector in SDK s32k1xx 15 does not execute correctly

When the program executes to the following code, the function cannot be executed

/* Calling flash command sequence function to execute the command */
ret = FLASH_DRV_CommandSequence(pSSDConfig);

0 项奖励
回复
1 回复

1,093 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Yang,

At first, I would like to ask you a few questions.

Which concrete MCU do you use?

Which SDK version and S32 Design Studio do you use?

What are the parameters such as the address and size of the erase sector function (FLASH_DRV_EraseSector)?

Can you share your code?

Thank you.

Best Regards,

Diana

0 项奖励
回复