CAN1 not work,CAN0 is ok

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN1 not work,CAN0 is ok

2,273 Views
wenzhuo_zhao
Contributor I

My mcu is S32K142_100lqfp。

CAN0 can work correctly。CAN0‘s transmission&reception is OK。

But CAN1 can not work。CAN1‘s TX can not ouput waveform。TX Pin output is high level

CAN1’s source code is similar with CAN0。

Program function is the status of the sending controller

0 Kudos
Reply
3 Replies

2,082 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

do you have CAN1 TX RX pin connected to transceiver and is the transceiver enabled? Try to disconnect CAN1 from transceiver and connect just MCU's TX/RX pins together and send a message. You should see CAN message transmitted still. This way you check if pins are properly configured. If there is no message visible, then you can have wrong CAN module pins initialization.

BR, Petr

0 Kudos
Reply

2,082 Views
wenzhuo_zhao
Contributor I

Hello, the Tx and Rx pins of CAN have a voltage of about 2.3V.

I don't know how to solve it. Can you help me?

0 Kudos
Reply

2,082 Views
wenzhuo_zhao
Contributor I

Thank you very much for your help.

I will try what you said.

0 Kudos
Reply