what is NXP's AUTOSAR OS for S32K?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what is NXP's AUTOSAR OS for S32K?

5,251件の閲覧回数
jianmin_zhou
Contributor II

I would like to know what is the name of NXP's AUTOSAR OS for S32K? 

if yes, which chip is supported by this OS? is S32k118 supported by this OS as well?

ラベル(1)
タグ(3)
0 件の賞賛
返信
4 返答(返信)

4,587件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I went through release notes and it looks like that also:

S32K118 MINI-MODULE S32K14XCVD-Q064 

and

S32K118 DEVICE 64LQFP PS32K118LAMLH 0N97V

is supported by AUTOSAR 4.2 sMCAL RTM 1.0.1 release.

Actually there are no more details about OS - there is only note that: 

It also includes an example of integration of the sMCAL drivers
with the NXP AUTOSAR OS/S32K v4.0.93 BETA v0.9.0 (the OS installer comes as a
different NXP software package).

Anyway - I'm not much familiar with autosar, you know, this community space is for S32 Design Studio support. 

Jiri 

0 件の賞賛
返信

4,587件の閲覧回数
cg0
Contributor II

Sorry, I know here is s32 DS, and recently i work on s32k autosar, do any s32k14x autosar documents, videos? thank you.

0 件の賞賛
返信

4,587件の閲覧回数
jianmin_zhou
Contributor II

Hi,

Is this AutoSAR MCAL, not AutoSAR OS?

On Tue, Jul 24, 2018 at 10:59 PM, [email protected] <[email protected]

0 件の賞賛
返信

4,587件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

from S32K family are supported by Autosar/MCAL S32K14x MCUs. Current version is Autosar 4.2.

Jiri 

0 件の賞賛
返信