s32ds ubuntu 18

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32ds ubuntu 18

2,199 次查看
mauriruizl81
Contributor I

 

Hello,

I have just follow the instruction to install s32ds in linux ubuntu 18, all steps, and special care in the java ones, but when I am executing the binary "S32DS.3.4_b201217_linux.x86_64.bin" I have got this error,

 

Preparing to install
Extracting the installation resources from the installer archive...
Configuring the installer for this system's environment...

Launching installer...

An internal LaunchAnywhere application error has occured and this application cannot proceed. (LAX)

Stack Trace:
java.lang.IllegalArgumentException: Malformed \uxxxx encoding.
at java.util.Properties.loadConvert(Properties.java:574)
at java.util.Properties.load0(Properties.java:391)
at java.util.Properties.load(Properties.java:317)
at com.zerog.common.java.util.PropertiesUtil.loadProperties(Unknown Source)
at com.zerog.lax.LAX.<init>(Unknown Source)
at com.zerog.lax.LAX.main(Unknown Source)

What could I do?

many thanks.

 

 

0 项奖励
回复
2 回复数

2,134 次查看
mauriruizl81
Contributor I

Hello, yes, sorry I found out what was going on, I had a string  "\u" in the PS1 environment variable, remove that and it went Ok. many thanks

2,136 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you met all the requirements for Linux OS mentioned in Install Guide (installing 32 libraries and so on)?

 

Jiri

0 项奖励
回复