newlib_nano under S32 DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

newlib_nano under S32 DS

1,909 Views
hanisamara
Contributor III

Hello,

i am trying to create a c++ project under S32DS for KEA128 Controller with newLib_nano no IO. But when i build the project (empty, just main) the code size is about 47k? did i miss anything to set? i did the same with a C Project and the code size is less than 1k?

thanks in advance,

Hani

2 Replies

1,792 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share your C++ project? I created new empty one for C++ with NewLib nano - and the code size is  less than 1kB:

pastedImage_1.png

Jiri

1,792 Views
hanisamara
Contributor III

Hello Jiri, 

thank you for your reply. I tried to update S32 DS and now it works correct and i have the same result as you. 

Thanks for your support, 

Hani

0 Kudos
Reply