having a single elf for multiple projects(application, bootloader , bootmanager)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

having a single elf for multiple projects(application, bootloader , bootmanager)

1,015件の閲覧回数
Tarek72
Contributor I

I'm currently trying to get a boot-manager/ bootloader/application to be linked as a single .elf file for the MPC5748G.

There are some issues that I'm a little confused about, and I would be very grateful if you could provide any guidance with regard to them.

The plan is to always boot the boot-manager and then jump to the application or the application according to the value of some flag. How to combine all 3 software entities into one instead of flashing each one on its own and if I manage to do that, would I be able to access the code of bootloader or application after jumping?

I have already defined different start and end addresses of each entity in the linker file and developed the jumping mechanism

0 件の賞賛
返信
1 返信

998件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信