error sending an activation request to a remote activation server and processing the resulting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error sending an activation request to a remote activation server and processing the resulting

4,208 Views
chai4896
Contributor I

error sending an activation request to a remote activation server and processing the resulting response.com. acresso. activation. handler. ServeException (FNP error 0)

0 Kudos
Reply
1 Reply

4,195 Views
mikedoidge
NXP Employee
NXP Employee

Hello Chai,

Have you tried to activate with Offline method?

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Activate-S32-Design-Studio/ta-p/...

It is possible that a firewall setting is blocking your PC from accessing the activation server. Sometimes this blocks the offline activation method, when performed from the same PC. You may need to use another PC, smartphone, tablet, or other device equipped with a web browser to perform the activation on the server, then transfer the resulting file to your PC for completion of the activation of S32 Design Studio.

Best Regards,

Mike