error: lto-wrapper failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error: lto-wrapper failed

3,318 Views
sarwath
Contributor IV

Hello,

I am getting this error: lto-wrapper failed while running the debug option.

Building target: MCSPTE1AK144_BLDC_6Step.elf
Invoking: Standard S32DS C Linker
arm-none-eabi-gcc -o "MCSPTE1AK144_BLDC_6Step.elf" "@MCSPTE1AK144_BLDC_6Step.args"
arm-none-eabi-gcc.exe: error: nano.specs: No such file or directory
lto-wrapper.exe: fatal error: C:\NXP\S32DS_ARM_v2.2\S32DS\build_tools\gcc_v6.3\gcc-6.3-arm32-eabi\bin\arm-none-eabi-gcc.exe returned 1 exit status
compilation terminated.
c:/nxp/s32ds_arm_v2.2/s32ds/build_tools/gcc_v6.3/gcc-6.3-arm32-eabi/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/real-ld.exe: error: lto-wrapper failed
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:63: MCSPTE1AK144_BLDC_6Step.elf] Error 1

16:09:30 Build Finished (took 19s.648ms)

sarwath_0-1661165082128.png

 

can anyone please help me on this.

BR,

Sarwath

0 Kudos
Reply
0 Replies