eabivle-gcc:MPU Opcodes not supported

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eabivle-gcc:MPU Opcodes not supported

1,930 次查看
bastian_schick
Contributor IV

Hi,

 

I use

gcc version 4.9.2 20141030 (Wed Sep 7 17:26:57 MSK 2016         build.sh rev= ELvle) (GCC)

 

It seems some opcodes are not support. At least those for the MPU:

mpuwe

mpusync

 

Also mas0  to mas3 are not known (minor problem, could add a #define).

 

I use these option for an MPC5744P:-mvle -mcpu=e200z4 -mspe2

Maybe I need to add something else?

 

Cheers

标签 (2)
0 项奖励
回复
1 回复

1,785 次查看
martin_kovar
NXP Employee
NXP Employee

Hello Bastian,

we know about this issue. Workaround is following. Use asm(".long 0xABCDABCD"). Instead of 0xABCDABCD use the opcode of the instruction you want to use.

Hope it helps.

Regards,

Martin