eCos or similar OS with bus support for MPC5748G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eCos or similar OS with bus support for MPC5748G

1,790 Views
tobiasfuelle
Contributor I

Hi,

 

I want to create a communication project on the MPC5748G by using its bus (CAN, LIN, FlexRAY) and its ethernet connection. Has anyone experienced a existing OS with available bus support? I prefer to use eCos, but as far as I know, it only exists for MPC56XX.

 

 

Kind regards,

 

Tobias

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,533 Views
martin_kovar
NXP Employee
NXP Employee

Hi Tobias,

you can use for example Autosar OS, which is available for MPC5748G. Autosar OS supports MCAL drivers for peripherals you want to use. If you want to use FlexRay, you will probably need Autosar OS. But this OS is not free, it is under license. Look at the following URLs:

http://cache.nxp.com/files/training/doc/dwf/DWF13_AMF_AUT_T0022.pdf?fsrch=1&sr=1&pageNum=1

AUTOSAR Software Solutions|NXP

Regards,

Martin

0 Kudos
Reply