build project 报错

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

build project 报错

1,404 次查看
showfaker66
Contributor II

showfaker66_0-1628497658913.png

我在编译时,然后报错,一直没找到原因,请求帮助,谢谢!

0 项奖励
回复
4 回复数

1,393 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

is it possible to share the project? Which version of S32 Design Studio is used?

Regards,

Lukas

0 项奖励
回复

1,384 次查看
showfaker66
Contributor II

Hi !

Each module was checked,no part was found to be occupied.

If it is convenient,how about I put up the project .Please help to have a look.

Thanks!

0 项奖励
回复

1,377 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

when you write a post here, you can find this below the text window:

lukaszadrapa_0-1628594701001.png

 So, you can easily attach the project here.

If it is confidential, you can create new ticket here and I will pick it up:

https://support.nxp.com/

Regards,

Lukas

 

0 项奖励
回复

1,324 次查看
showfaker66
Contributor II

Hi

The problem has been solved.

I rebuilt an empty project, and then got the code and the corresponding configuration.

And now we're ready to run.

Thanks!

 

0 项奖励
回复