Why the format of MAP from S32 Design Studio generation diffierent from the MAP generation from Other compiler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why the format of MAP from S32 Design Studio generation diffierent from the MAP generation from Other compiler

1,356 Views
edenli
Contributor V

Hi Guys,

I use the S32 compiler to generate the MAP file shown as the attchment named A.map,

and  the other compiler is named B.map,

how can i make the fromat of the  A to the format that B.map? 

Original Attachment has been moved to: B.map.zip

Original Attachment has been moved to: A.map.zip

0 Kudos
Reply
1 Reply

1,150 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

I'm afraid that you can't simply convert gcc/ld map file output format to format of Texas Instrument map file.  

If you need the "B" format as an input for parser - you have to modify your parser to be able handle gcc/ld map file format. 

Jiri

0 Kudos
Reply