Unable to resolve Semantic errors in S32 design studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to resolve Semantic errors in S32 design studio

Jump to solution
3,269 Views
Anilpatil_SasvaAuto
Contributor III

Hello Team,

I am trying to compile the NFC reader library project. After a successful build, I did not encounter any compilation errors or warnings; however, I found two semantic errors in the Problems window.

These errors appear even after I have provided the path to include in the IDE settings. Please note that these errors will not be displayed in the Problems window unless you open the "phbalReg_S32kSpi.c" file from the DAL folder.

Please refer to the attached files for your reference

I would appreciate any solutions to resolve the symbols or errors. Thank you!

0 Kudos
Reply
1 Solution
3,002 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

I'm not able reproduce the issue. Can you please share the screenshot with the errors and ideally with error details if there are some? 

View solution in original post

0 Kudos
Reply
6 Replies
2,534 Views
Anilpatil_SasvaAuto
Contributor III

Issue resolved from my side

 

0 Kudos
Reply
3,254 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

what's your S32DS version and target MCU? 

0 Kudos
Reply
3,231 Views
Anilpatil_SasvaAuto
Contributor III
S32DS version: 3.4
Target MCU:S32K144EVB
0 Kudos
Reply
3,216 Views
jiri_kral
NXP Employee
NXP Employee

And which particular version of NFC Reader library are you using? 

0 Kudos
Reply
3,184 Views
Anilpatil_SasvaAuto
Contributor III

NFC reader library version number: aNfcRdLib_SDK_Evaluation_v2.28

0 Kudos
Reply
3,003 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

I'm not able reproduce the issue. Can you please share the screenshot with the errors and ideally with error details if there are some? 

0 Kudos
Reply