There was a problem about Change Vision SDK root in S32DS for Vision

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

There was a problem about Change Vision SDK root in S32DS for Vision

1,657 Views
xiao_yongguo
Contributor I

Installed S32 Design Studio for Vision v2.0, embedded SDK V1.0.0,.

I feel that the version V1.0.0 is too old, I installed a new version of SDK V1.2.0,  and according to the S32DS manual "

Change Vision SDK root in S32DS for Vision.pdf” Replace and associate a new version of the SDK path:
pastedImage_1.png
When creating example, an error occurred while generating the code: the prompt file does not exist:
pastedImage_2.png
If you restore S32DS_VSDK_DIR to the old version embedded, you can successfully operate.
Now confirm that the new version of SDK V1.2.0 installation is no problem, the DEMO files is complete.
I don't know what's going on, Request help, thank you!
Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,505 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

S32DS for Vision v2.0 supports VSDK RTM 1.0.0. If you update SDK, some examples may not work. 

If you need new VSDK, you can use it from command line without S32DS for Vision. 

Jiri

0 Kudos
Reply

1,505 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

please use English language. We are world wide community. Thank you. 

Jiri 

0 Kudos
Reply