S32ds 3.4 Linux debug problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32ds 3.4 Linux debug problem

2,865件の閲覧回数
FaustoPignatta
Contributor I
Hi,
I debug my s32k148 application with USB-Multilink in windows without problem.
But if I try it in Linux (Ubuntu) S32DS doesn't see any debugger connected.
I've downloaded and installed Linux drivers provided by pemicro.
Some ideas to resolve this issue?
Thanks

Fausto
0 件の賞賛
返信
3 返答(返信)

2,836件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Fausto, 

are you using virtual machine or real one? Is the PE Micro listed if you run lsusb command? 

 

Jiri

0 件の賞賛
返信

2,692件の閲覧回数
FaustoPignatta
Contributor I

I'm using virtual machine. Yes Pe mricro is listed when I try lsusb command.

Thanks

0 件の賞賛
返信

2,784件の閲覧回数
MateoSegura413
Contributor III

@jiri_kral I am having the same issue. Yes the device shows up under lsusb. Could you give me some guidance as to how I can use the PE micro debugger under linux?

Thanks in advance!

 

0 件の賞賛
返信