S32V234 2x Video interface unit (VIU) for camera input

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32V234 2x Video interface unit (VIU) for camera input

2,848件の閲覧回数
adnan
Contributor I

Hello,

I would like to know about the 2x Video interface unit (VIU) for camera input available on the S32V234 SoC. What kind of input format does these two interfaces support? Does these interfaces support camera input in the following format? 8-Bit Parallel in BT.656 format? Please check the attached picture

Thank you

タグ(1)
0 件の賞賛
返信
1 返信

2,795件の閲覧回数
bpe
NXP Employee
NXP Employee

Please be aware, that support to S32V234 Vision subsystem  is
done only via tickets. This Community is not appropriate for questions
of this kind. If you wish to receive feedback from NXP Technical Support
with respect to this question, please open a Support Case.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信