S32R274rruevb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R274rruevb

2,357 Views
220141204
Contributor I

Hi,

I have ordered the part S32R274RRUEVB (daughter board only). I would like to know:

(1) Is it possible to load program / run / debug use the daughter board only?

(2) If it is, what connection is necessary between daughter board and PC? For example, from a question (https://community.nxp.com/message/1037532?q=S32R274rruevb) I knew that PE Micro USB Multilink is recommended for connection, but what Micro USB Multilink do?

(3) Furthermore, is a USB mini cable able to meet my requirements(debug/load/run), or if I could do it with a USB mini calbe plus a JTAG debugger?

Thanks in advance!

0 Kudos
Reply
1 Reply

1,939 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes, the Daughter board can be used as standalone EVB. You need external power supply 5V, 3.3V and 1.25V. 

There is no OpenSDA debug probe present on board. Mini USB connector is used as RS232 over USB. You have to use external debug probe - PE Micro Multilink FX for example.

Hope it helps. 

Jiri