S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,261件の閲覧回数
乔国栋
Contributor II

The creation project will wait for execution to fail

b306d2e23e060f7be977ef3b3bfa630.jpg

What is the cause and how can I solve it?

0 件の賞賛
返信
1 解決策
2,234件の閲覧回数
乔国栋
Contributor II

It was normal before, now it is normal, I re-downloaded S32DS for ARM, and it is normal.I didn't save the log

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,243件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

Was the S32 Design Studio working normally before? Or is this issue happening at the first time you used it?

If it is first time, could you please share the installation log file? (ex. C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs)

Also, please check the workspace directory folder '.metadata' and send us the file '.log'.

Best Regards,

Mike

0 件の賞賛
返信
2,234件の閲覧回数
乔国栋
Contributor II

It was normal before, now it is normal, I re-downloaded S32DS for ARM, and it is normal.I didn't save the log

0 件の賞賛
返信