S32DS installation DIAB compiler programming error problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS installation DIAB compiler programming error problem

3,900 Views
lubo_NEW
Contributor III

The same project compiled with DEBUG and DEBUG RAM has different content

1111.png2222.png

0 Kudos
Reply
6 Replies

3,889 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks, that in linker file script for RAM target are not defined symbols mentioned in linker errors. It is possible share your project? 

 

Jiri 

0 Kudos
Reply

3,876 Views
lubo_NEW
Contributor III
Spoiler
 
0 Kudos
Reply

3,868 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

it looks that you aren't using memory.dld linker script file for _RAM target. Unfortunately I don't have DIAB compiler on my machine and can't test it. Please check the differences in Project properties -> Linker settings for Debug and RAM target. The memory.dld is the clue. 

 

Jiri 

0 Kudos
Reply

3,850 Views
lubo_NEW
Contributor III

Thank you for your reply. Could you please help me to see what the problem is with another mistake as shown in the picture11111.png

0 Kudos
Reply

3,831 Views
stanish
NXP Employee
NXP Employee

Hi lubo,

The problem you observe with Debug RAM build is that there are sections in the Debug Configuration (Flash) that are not present in RAM build (typically reset vector section, ROM->RAM copy sections,...)

Since your Debug (Flash) build configuration project startup routines rely on custom linker symbols that contain e.g addresses or of these sections (OS_NONCACHE_BSS_START...) - these symbols are missing for RAM configuration.

You need to define these symbols in 57xx_ram.dld linker file and probably use conditional compilation to skip startup ROM->RAM copy-down routines for RAM project.

Hope it helps.

Stan

0 Kudos
Reply

3,899 Views
lubo_NEW
Contributor III

Why does Debug compile not produce an error, while Debug RAM compile does

0 Kudos
Reply