S32DS for ARM 2018 R1_operate S32DS by command line completely on server _FC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS for ARM 2018 R1_operate S32DS by command line completely on server _FC

Jump to solution
3,112 Views
Fidel
Contributor IV

Dears,

        now a S32DS for ARM 2018 R1 is installed on a server, the server with a linux server OS without any GUI, so is it possible to operate the S32DS completely by command line? cause no GUI ,so I cannot operate it just by clicking here and there.

 

0 Kudos
Reply
1 Solution
3,089 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes, that's correct. S32DS requires Window manager for installation - it can't be done from console only. 

 

The solution can be to use standalone gcc for ARM and write your own makefile for your project.  

View solution in original post

0 Kudos
Reply
4 Replies
3,101 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

Yes, command line is supported. Please see this article:

HOWTO: S32 Design Studio Command Line Interface

Best Regards,

Mike

0 Kudos
Reply
3,099 Views
Fidel
Contributor IV

Hi Mike,

         I look what you mentioned, but I found that that is on the condition that the Eclipse was installed correctly ,but now our real situation is that we want to do all the operation on the linux server OS, that means even the Eclipse cannot be installed , that is right? so the following operation you mention all cannot be done, that is right? so in a word , there is no way to operate S32DS all by command line on Linux Server, that is right?

0 Kudos
Reply
3,090 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes, that's correct. S32DS requires Window manager for installation - it can't be done from console only. 

 

The solution can be to use standalone gcc for ARM and write your own makefile for your project.  

0 Kudos
Reply
3,088 Views
Fidel
Contributor IV

got it ,thx~

0 Kudos
Reply