In S32DS for the MPC5775K, three separate projects are created, one for each core (foo_Z4_1, foo_Z7_2, foo_Z7_3). When the workspace is built, three separate .elf files are generated, one for each project (foo_Z4_1.elf, foo_Z7_2.elf, foo_Z7_3.elf). This is all fine, and I can download and debug on our test board.
We also have the P&E Micro PROGPPCNEXUS utility which will erase and program .elf files to the MPC5775K. However, it will only accept a single .elf file.
I was wondering if there were built-in tools within S32DS to automatically merge the three project .elf files into a single .elf for use with the PROGPPCNEXUS tool, or if that was something we'd have to do on our own. E.g. "foo.elf" from the three "foo_XY_Z.elf" files. I didn't see anything immediately obvious in the documentation nor help for S32DS.
Thanks in advance,
Joe Shidle