S32DS ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS ERROR

3,347 Views
347996379
Contributor III

S32DS error.png

This problem occurs when I build my project.

why?

0 Kudos
Reply
6 Replies

3,041 Views
BlackNight
NXP Employee
NXP Employee

It seems that either your toolchain is not configured properly or that maybe a virus scanner has removed your binaries. Can you check that all the needed files are present in the bin folder?

pastedImage_1.png

Other than that, I recommend that you create a new project with the wizard and to see if the problem is with your project or with your setup. Or that you share/upload your project.

I hope this helps,

Erich

0 Kudos
Reply

3,041 Views
347996379
Contributor III
  • When I create a new S32K148 project, it's ok to compile and run,maybe there is something wrong whit my project configuration, could you take a look at it for me? sorry ,but I don't how to add file(project) to the NXP.

0 Kudos
Reply

3,041 Views
BlackNight
NXP Employee
NXP Employee

So there is definitely something wrong with your project.

You can upload your project the same way as you uploaded your previous zip file.

I suggest you compare your project settings with the one working, you probably can spot the difference easily.

Or you can compare the .cproject files inside your project root.

I hope this helps,

Erich

0 Kudos
Reply

3,041 Views
347996379
Contributor III

hello,I've already offered my project. Can you take a look at it for me?

0 Kudos
Reply

3,041 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

there was wrong toolchain in your project - just choose the correct one in project properties. 

pastedImage_1.png

After that - GNU tools can be found. 

Hope it helps. 

Jiri 

0 Kudos
Reply

3,036 Views
347996379
Contributor III

Please take a look at it for me ,thanks!

0 Kudos
Reply