S32DS Activation Failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Activation Failure

4,740 Views
JayceYang
NXP Employee
NXP Employee

Hi ,

I got an error when tried to activate S32DS_v3.2 for S32G2:

nxf65134_0-1602208398573.png

I want to install S32DS_v3.2, but installed and activated S32DS_v3.3 before installing S32DS_v3.2. Now I can't activate S32DS_v3.2. I am already uninstalled S32DS_3.3, but it's still not working.

Could you please help me with this problem?

 

Thanks & Regards,

0 Kudos
Reply
6 Replies

4,730 Views
mikedoidge
NXP Employee
NXP Employee

Hello @JayceYang,

To resolve this, please try the following to reset the trusted storage:

Windows host:

-> Delete 'C:\ProgramData\FLEXNet'

 

This folder may be hidden by default, so then it would be necessary to change Windows Explorer settings to show hidden items.

Linux host:

/usr/local/share/macrovision/storage

 

Let us know if the issue is still not resolved.

Mike

0 Kudos
Reply

4,716 Views
JayceYang
NXP Employee
NXP Employee

Hi Mike,

Thanks for reply, but it's still not work.

After deletion of the folder FLEXNet, and trying to activate S32DS_v3.2 again:  (1)

 

WeChat Image_20201010160353.png

Click "ok", then :   (2)

WeChat Image_20201010160406.png

Click "Online" and input activation code, then it comes back to (1) again.

Stuck in this loop, unable to move forward.

 

 

 

 

0 Kudos
Reply

4,691 Views
mikedoidge
NXP Employee
NXP Employee

@JayceYang,

Please try selecting 'OK' to return the license, and try again, it should allow you to activate. It needs to complete the process of returning the previous license before it will allow you to activate this one.

Mike

0 Kudos
Reply

4,671 Views
JayceYang
NXP Employee
NXP Employee

Clicked ‘OK‘, completed the process of returning and then inputted activation code again. Just back to this “return step” as I showed in the last reply.

0 Kudos
Reply

4,655 Views
mikedoidge
NXP Employee
NXP Employee

Hello @JayceYang,

What activation code are you using? I have checked your account, but I find that only 'S32 Design Studio for ARM' and 'S32 Design Studio for PA', but there is no 'S32 Design Studio v3.3' nor for 'v3.2'. I suggest that you register this product to your account and then use the activation code which is correct for this product. Here is the direct link for S32 Design Studio for S32 Platform v3.2

Once you have tried the new activation code, please let us know the result.

Mike

0 Kudos
Reply

4,643 Views
JayceYang
NXP Employee
NXP Employee

Hi Mike,

Thanks for help.

I've successfully installed it.

0 Kudos
Reply