S32DS Activation Failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS Activation Failure

4,701件の閲覧回数
JayceYang
NXP Employee
NXP Employee

Hi ,

I got an error when tried to activate S32DS_v3.2 for S32G2:

nxf65134_0-1602208398573.png

I want to install S32DS_v3.2, but installed and activated S32DS_v3.3 before installing S32DS_v3.2. Now I can't activate S32DS_v3.2. I am already uninstalled S32DS_3.3, but it's still not working.

Could you please help me with this problem?

 

Thanks & Regards,

0 件の賞賛
返信
6 返答(返信)

4,691件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @JayceYang,

To resolve this, please try the following to reset the trusted storage:

Windows host:

-> Delete 'C:\ProgramData\FLEXNet'

 

This folder may be hidden by default, so then it would be necessary to change Windows Explorer settings to show hidden items.

Linux host:

/usr/local/share/macrovision/storage

 

Let us know if the issue is still not resolved.

Mike

0 件の賞賛
返信

4,677件の閲覧回数
JayceYang
NXP Employee
NXP Employee

Hi Mike,

Thanks for reply, but it's still not work.

After deletion of the folder FLEXNet, and trying to activate S32DS_v3.2 again:  (1)

 

WeChat Image_20201010160353.png

Click "ok", then :   (2)

WeChat Image_20201010160406.png

Click "Online" and input activation code, then it comes back to (1) again.

Stuck in this loop, unable to move forward.

 

 

 

 

0 件の賞賛
返信

4,652件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

@JayceYang,

Please try selecting 'OK' to return the license, and try again, it should allow you to activate. It needs to complete the process of returning the previous license before it will allow you to activate this one.

Mike

0 件の賞賛
返信

4,632件の閲覧回数
JayceYang
NXP Employee
NXP Employee

Clicked ‘OK‘, completed the process of returning and then inputted activation code again. Just back to this “return step” as I showed in the last reply.

0 件の賞賛
返信

4,616件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @JayceYang,

What activation code are you using? I have checked your account, but I find that only 'S32 Design Studio for ARM' and 'S32 Design Studio for PA', but there is no 'S32 Design Studio v3.3' nor for 'v3.2'. I suggest that you register this product to your account and then use the activation code which is correct for this product. Here is the direct link for S32 Design Studio for S32 Platform v3.2

Once you have tried the new activation code, please let us know the result.

Mike

0 件の賞賛
返信

4,604件の閲覧回数
JayceYang
NXP Employee
NXP Employee

Hi Mike,

Thanks for help.

I've successfully installed it.

0 件の賞賛
返信