S32DS_ARM_v2018.R1's examples project: KEA128/bootloader_KEA is not run after reset?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS_ARM_v2018.R1's examples project: KEA128/bootloader_KEA is not run after reset?

1,882件の閲覧回数
chenaimei15
Contributor I

Hi,why  S32DS_ARM_v2018.R1's examples project:  KEA128/bootloader_KEA is not run after reset?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,626件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi may 王,

Sorry for my late reply!
I am not sure if you have following the steps in description.
The RAppID BL Tool can be download from here.
The rbf file is under the install folder of this tool .(C:\Freescale\RAppIDBL\RBF_Files)

bootloader_KEA.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,626件の閲覧回数
chenaimei15
Contributor I

Hi  Robin:  Thank you for  your information。I  will learn to use the RAppID Boot Loader Utility  later。

0 件の賞賛
返信