S32DS_ARM_v2018.R1's examples project: KEA128/bootloader_KEA is not run after reset?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS_ARM_v2018.R1's examples project: KEA128/bootloader_KEA is not run after reset?

1,885 Views
chenaimei15
Contributor I

Hi,why  S32DS_ARM_v2018.R1's examples project:  KEA128/bootloader_KEA is not run after reset?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,629 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi may 王,

Sorry for my late reply!
I am not sure if you have following the steps in description.
The RAppID BL Tool can be download from here.
The rbf file is under the install folder of this tool .(C:\Freescale\RAppIDBL\RBF_Files)

bootloader_KEA.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,629 Views
chenaimei15
Contributor I

Hi  Robin:  Thank you for  your information。I  will learn to use the RAppID Boot Loader Utility  later。

0 Kudos
Reply