Hello,
After downloading the S32DS 3.3 for S32K3 we tried to activate the software “online” using the activation code 62EB-2992-3A9E-5720. This was not successful, so we tried the offline activation method. Below you find activation request file generated. As you can see, the correct activation code is listed in this file.
<?xml version="1.0" encoding="UTF-8"?>
<Request xmlns="http://www.macrovision.com/fnp/2004/11/activation"><RequestHeader><VersionNumber>3</VersionNumber><RequestType>ACTIVATION</RequestType></RequestHeader><RequestData><EntitlementData><EntitlementId>62EB-2992-3A9E-5720</EntitlementId><ActivationReason>0</ActivationReason><ProductId>Not Applicable</ProductId><PublisherId>10295808</PublisherId></EntitlementData><OriginData><ClientVersion>11.13.0</ClientVersion><ConfigData><IsServer>0</IsServer><TrustedHostInformation><TrustedId>3</TrustedId><Revision>1</Revision><RevisionType>SRV</RevisionType><MachineIdentifier>3F86BF0C8E8B4D3E588AB8E81EA141DEDBC0935D</MachineIdentifier><Status>OK</Status></TrustedHostInformation></ConfigData><Platform><PlatformTypeName>x64_n6</PlatformTypeName><OperatingSystem><Info>none</Info></OperatingSystem></Platform><UniqueMachineNumbers><UniqueMachineNumber><Type>1</Type><Value/></UniqueMachineNumber><UniqueMachineNumber><Type>2</Type><Value>BFE4B29080DD51DEA96ABE11C9651F043580A0CA</Value></UniqueMachineNumber></UniqueMachineNumbers><SequenceNumber>4</SequenceNumber></OriginData><PublisherDictionary><Entries><Entry><Key>flexFulfillmentVersion</Key><Value>1</Value></Entry></Entries></PublisherDictionary></RequestData><Hash>FF3F2E18D20B1A8E0223F89540CD959A6A20B45A</Hash><HashVersion>1</HashVersion></Request>
When we tried to activate using the responsfile, we get an error message. If you look at the activation response file below, you see, that there is also an error message within this file:
<?xml version="1.0" encoding="UTF-8"?>
<Response xmlns="http://www.macrovision.com/fnp/2004/11/activation"><ResponseHeader><VersionNumber>1</VersionNumber><ResponseType>FAILURE</ResponseType><RequestSequenceNumber>7</RequestSequenceNumber><RequestHash>A5AA60F617BCBF0F06C8455A52A61F67D4A97F2B</RequestHash></ResponseHeader><ResponseData><ResponseReason>ERROR</ResponseReason><ErrorCode>A unique license definition and a unique license variation could not be determined for this product and entitlement line.</ErrorCode></ResponseData><Signature>A32BD0CE356DBED26DE72CF46316F39D6362BD6B</Signature><SignatureVersion>1</SignatureVersion></Response>
we followed the instruction from the following website:
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Activate-S32-Design-Studio/ta-p/...
Any idea what the problem could be and how we can solve this?
Best Regards
Roger