S32 for Power - Compatibility with NXP Motor Control Toolbox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 for Power - Compatibility with NXP Motor Control Toolbox

Jump to solution
3,919 Views
chosp
Contributor III

Hello

 

We are successfully developing on the MPC5744P using S32 Design Studio and PE Multilink.

The NXP Motor Control Toolbox for MATLAB was downloaded for evaluation purposes, but the S32 toolchain is not available among the configurable toolchain choices regarding code generation.

 

Is support for the S32 IDE planned? If yes, do you have an approximate timeline?

 

Thank you

Labels (1)
1 Solution
3,727 Views
PatrickMenter
NXP Employee
NXP Employee

The support for the MC Toolbox for MPC5744P to support the GCC compiler in S32 Design Studio is planned for later this year. The larger target plan is to add this support in late Q3 or early Q4.

View solution in original post

1 Reply
3,728 Views
PatrickMenter
NXP Employee
NXP Employee

The support for the MC Toolbox for MPC5744P to support the GCC compiler in S32 Design Studio is planned for later this year. The larger target plan is to add this support in late Q3 or early Q4.